Tool News
 
 
 

Tool News

Products Info
Downloads
Tools FAQs
MESC TOOL NEWS: MESCT-CC32R_1-000316D

CC32R V.2.10 Release 1
Upgraded Version Announcement

This is to announce that cross-tool kit CC32R for the M32R family of microcomputers has been upgraded from its V.2.00 Release 1 to V.2.10 Release 1.


  1. Descriptions of Upgrade
    1.1 Function introduced
    An option of "-warn_suppress_code_data" has been introduced to suppress the display of warning message "warning:caution!there are some data in code section". This message appears when data is placed in a code section.

    1.2 Known problems fixed
    The following known problems have been fixed:
    (1) Changing output directories of an object etc. results in link errors when TM (Integrated Development Environment) is used.
    For details refer to "CC32R V.2.00 Release 1 Precaution" issued on September 16, 1999.

    (2) When compiling C-language source files, codes that compare incorrect bit positions are generated so that wrong conditional branches may occur.
    For details refer to "CC32R Precaution" issued on October 16, 1999.

    (3) When executing switch statements in C-language source files, incorrect case labels may be selected.
    For details refer to "CC32R Precaution" issued on December 16, 1999.



  2. How To Upgrade CC32R
    Upgrading procedure varies according to the version of your product.
    2.1 For the customer who has their license ID (Using CC32R V.1.00 Release 4 or later)
    (1) Please download the upgraded product without charge from HERE.

    (2) Upgrade by CD-ROM with additional charge
    When ordering, be sure to enter "-VUP" in the Comment column. The license ID is not needed to enter.
    Example: W95E-VUP

    2.2 For the customer who has their Serial No. (Using CC32R V.1.00 Release 3 or earlier)
    (1) Obtaining a license ID (without charge)
    Fill in the appended "Free-of-Charge CC32R License ID Application Form" and send it to your local Renesas Technology sales office or distributor by E-mail. We will inform you of your license ID by return.
    Then, download the upgraded product by using it from HERE.
    Note that your newly obtained license ID is not a temporary one for this online upgrade.

    (2) Upgrade by CD-ROM with additional charge
    When ordering, be sure to enter "-VUP" and your Serial No. in the Comment column.
    Example: W95E-VUP-Serial No.

    [Notice]
    * The upgrade is available only to customers who have sent their customer registration card to us by mail or fax.
    * Since the publication of the IBE version has been discontinued from V.1.00 Release 4, please upgrade your product to the W95E version, if necessary.
    * After this upgrade our support for the product will be provided on your license ID, not your Serial No.


    2.3 First ordering or upgrade by CD-ROM

    Ordering Information
    ComputerOSType NameComment
    IBM PC/AT
    or
    compatible
    Windows 98
    Windows 95
    Windows NT 4.0
    M-CC32RFor first ordering:W95E
    For upgrading:W95E-VUP-[Serial No.]
    * Serial No. is not needed to enter if you have your license ID.






© 2008. Renesas Technology Corp., All rights reserved. Privacy | Legal