Tool News
 
 
 

Tool News

Products Info
Downloads
Tools FAQs
MESC TOOL NEWS: MESCT-M16C/62POD-000416D

Precautions Concerning to Emulation Pods
for M16C/62, 6H, and 6N Groups
and Compact Emulator for M16C/62 Group MCUs

Please take note of the following problem in using pullup control registers of the emulation pods for the M16C/62, 6H, and 6N groups and the compact emulator for the M16C/62 group MCUs.


  1. Products Concerned
    Product TypeSerial Numbers
    M30620T-RPD-EAll the serial numbers
    (includingremodeled products for M16C/62A)
    M30620TB-RPD-EAll the serial numbers
    (including remodeled products for M16C/62A)
    M30620T2-RPD-EAll the serial numbers
    M30600T-RPD-ERemodeled products for M16C/62 only
    M30610T-RPD-ERemodeled products for M16C/62 only
    Emulation Pod for
    M16C/6H Group MCUs
    (Specific Product)
    All the serial numbers
    Emulation Pod for
    M16C/6N Group MCUs
    (Specific Product)
    All the serial numbers
    M30620T-CPE
    (Compact Emulator for M16C/62 Group MCUs)
    All the serial numbers

    Note:The following products are not concerned in this problem:
    * M30600T-RPD-E (not remodeled for M16C/62 group MCUs)
    * M30610T-RPD-E (not remodeled for M16C/62 group MCUs)
    * Emulation pod for M16C/6K group MCUs
    * Emulation pod for M16C/6V group MCUs


  2. Problem
    When pull-up control register 1 for port pins P44--P47 (bit 1 of address 3FDh: PU11) is set to "1" (pulled up), port pins P15--P17 are also pulled up regardless of the setting of pull-up control register 0 for port pins P14--P17 (bit 3 of address 3FCh: PU03).
    However, this problem arises only in the emulation pods and compact emulator listed above and does not arise in actual MCUs.

    Status of PU03Status of PU11Port Pins P15--P17
    00Not pulled up
    10Pulled up
    01Pulled up (*1)
    11Pulled up

    *1: Not pulled up in actual MCUs.

  3. Cause
    Please be aware that this problem is inherent to the specifications in the emulate mode of MCUs. Therefore, when using pull-up control register 1 for port pins P44--P47 (bit 1 of address 3FDh: PU11), it should be noted that different operations can be observed from those in actual MCUs.




© 2008. Renesas Technology Corp., All rights reserved. Privacy | Legal