Tool News
 
 
 

Tool News

Products Info
Downloads
Tools FAQs
MESC TOOL NEWS: MESCT-SRA74-000416D

Precaution
Concerning to CV74 Included with SRA74

Please take note of the following problem in using CV74, the file conversion tool for the M37280 MCU, included with SRA74:


  1. Version Concerned
    File conversion tool for the M37280 MCU
    CV74 V.1.00.00
    included with SRA74 V.4.00 Release 1 or later (relocatable assembler with integrated development environment for the 740 family MCUs)

  2. Problem
    When a line with 256 or more characters including a new line character exists in the symbol file that has not already been converted by CV74, the file may not be read into the debugger after converted by CV74.

  3. Workaround
    In advance of invoking CV74, insert a hard return into a line with 256 or more characters to make it a shorter line within 255 characters. Be sure, at this time, to place a hard return immediately before a symbol or label name.

  4. Schedule of Fixing Problem
    We plan to fix this problem in our next release.



© 2008. Renesas Technology Corp., All rights reserved. Privacy | Legal