Tool News
 
 
 

Tool News

Products Info
Downloads
Tools FAQs
MESC TOOL NEWS: MESCT-MM-000516D

MM V.2.00.20
Upgraded Version
Announcement

This is to announce that mask file utility MM for the Mitsubishi MCUs has been upgraded from its V.2.00.10 to V.2.00.20.


  1. Function Introduced
    When mask ROM patterns are created from the machine language file of the user program and the OSD font data, it is necessary to choose a font data file by entering its filename in "OSD:". At this choice, the new version displays the following confirmation messages:

     ------------------------------------------------------------------------
       Mitsubishi Mask-ROM File Maker V.2.00.20
       Copyright 2000, MITSUBISHI ELECTRIC CORPORATION
       AND MITSUBISHI SEMICONDUCTOR SYSTEMS CORPORATION
       All Rights Reserved.
    
       Rom Data file name ?    
       Return-key to end data entry
       OSD:SAMPLE.HEX
    
       Specification of 'OSD:' can use only the microcomputer with OSD function.
       Do not specify 'OSD:' by the kind without OSD function.
       If it is specified as the kind without OSD function,
       mask processing cannot be carried out correctly.
       Refer to the 'Mask ROM Confirmation Form' for whether the kind which you 
       use corresponds.
       May it specify? (When implementing, you input Y and Enter key)
       -->      
       ------------------------------------------------------------------------
    
    This function prevents font data files from inadvertently being chosen on MCUs not provided with OSD function.

  2. How to Upgrade
    Online upgrade is available without charge. Please download the upgraded product from HERE.






© 2008. Renesas Technology Corp., All rights reserved. Privacy | Legal