|
|
 |
MESC TOOL NEWS:
MESCT-PD308-000516D
PD308, PD30, PD79, PD77, PD38
Precautions
|
Please take note of the following problem in using emulator debugger PD308, PD30, PD79, PD77, and PD38:
-
Versions Concerned
| PD308 V.2.00 Release 1 | for the M16C/80 series MCUs |
| PD30 V.5.00 Release 1 | for the M16C/60,M16C/20 series MCUs |
| PD79 V.3.00 Release 1 | for the 7900 series MCUs |
| PD77 V.3.00 Release 1 | for the 77xx series MCUs |
| PD38 V.4.00 Release 1 | for the 740 family MCUs |
-
Problem
If the Line Assemble dialog box is closed with the NOP check box being checked, the emulator debugger won't work correctly. (This problem will not occur if the Line Assemble dialog box is not already opened.)
[Example]
(1) Even when '0' is set to the registered bit symbol (or a set of an address and bit number) in ASM watch window, '1' will be displayed.
(2) When '0' is set to a bit symbol by BIT command, an error will arise (ERROR 2600: a syntax error in the command line).
-
Workaround
Be sure to uncheck the NOP check box when closing the Line Assemble dialog box.
-
Schedule of Fixing Problem
We plan to fix this problem in our next release.
|
 |