Tool News
 
 
 

Tool News

Products Info
Downloads
Tools FAQs
MESC TOOL NEWS: MESCT-RASM77-000616D

LST77 and LST74
Precautions

Please take note of the following problem in using absolute address list creation tools LST77 for the 77xx series and LST74 for the 740 family of microcomputers:


  1. Versions Concerned
    LST77 V.1.00.00 included with compiler NC77WA and assembler RASM77
    LST74 V.1.00.00--V.1.02.00 included with assembler SRA74
    * Old versions of both LST77 and LST74 in which characters of C, S, etc. are appended to their version numbers, for example, V.1.01.00C, are also concerned with this problem.

  2. Problem
    At typing a command, selecting only an option without specifying the name of a file to convert will force termination of LST77 or LST74.
    [Example of Typing a Command]
    ----------------------
     >LST74 -Od:\tmp
    ----------------------
    

  3. Workaround
    Be sure to specify the name of a file to convert. In the above example, if you want to name a file output.sym, and output.hex, type a command as follows:
    ------------------------
     >LST74 output -Od:\tmp
    -------------------------
    

  4. Schedule of Fixing Problem
    We plan to fix this problem in our next release.






© 2008. Renesas Technology Corp., All rights reserved. Privacy | Legal