Tool News
 
 
 

Tool News

Products Info
Downloads
Tools FAQs
MESC TOOL NEWS: MESCT-PCA4738H-100A-000716D

Announcement of a New MCU
Supported by PCA4738H-100A

This is to announce that a new MCU has been added to the line supported by programming adapter PCA4738H-100A (used with a 100-pin 0.4-mm-pitch TQFP package) for the 38000 series of MCUs.


  1. Product Concerned
    Product TypeNew MCU
    PCA4738H-100AM37528EAHP


  2. Settings at Programming
    The settings of PCA4738H-100A and a PROM programmer at programming the ROM in the M37528EAHP are as follows:
    (1)Recommendable PROM programmer: R4945 or R4945A (manufactured by Advantest Corp., Japan)

    (2) PROM programmer's mode for programming: M5M27C101 mode (byte write)

    (3)Switch settings of PCA4738H-100A:

    SW1SW2SW3
    CMOSCMOSOFF

    (4)Area settings:

    Programming Area in PROM Programmer ROM Area in MCU
    0608016 -- 0FFFD16608016 -- FFFD16



© 2008. Renesas Technology Corp., All rights reserved. Privacy | Legal