Tool News
 
 
 

Tool News

Products Info
Downloads
Tools FAQs
MESC TOOL NEWS: MESCT-PD79SIM-000716D

PD79SIM V.3.10 Release 1
Upgraded Version Announcement

This is to announce that simulator debugger PD79SIM for the 7900 series MCUs has been upgraded from its V.3.00 Release 1 to V.3.10 Release 1.


  1. Descriptions of Upgrade
    1.1 Problems Fixed
    The following known problems have been fixed:
    (1) In the ASM watch window, modifying memory data by using watch points of 2 or 4 bytes wide beginning at an odd address may cause communication protocol errors to occur.
    For details refer to TN-2 "Precaution in Using Simulator Debuggers for 16-Bit MCUs" issued on December 1, 1999.
    (2) Subtract operations in the decimal mode will incorrectly be performed.
    For details refer to TN-4 "PD79SIM and PD77SIM Precautions" issued on April 16, 2000.
    (3) Clicking the MPL button in the MR window may display Windows' error message "This program has performed an illegal operation. . . ."
    For details refer to TN-2 "PD308SIM, PD308, PD30SIM, PD30, PD79SIM, and PD79 Precautions" issued on June 1, 2000.
    (4) During display of the Source dialog box in the Program or Source window (opened by using View -> Source button or menu), Windows' error message appears, forcing termination of the program.
    For details refer to TN-2 "PD32RSIM, PD308SIM, PD30SIM, PD79SIM, PD77SIM, PD32000, PD308, PD30, PD79, PD77 Precautions" issued on June 16, 2000.


  2. How to Upgrade Current Products and Order Upgraded Ones
    2.1 Online Upgrades (without Charge)
    Please download the upgraded product from HERE.

    2.2 First Ordering or Upgrading by CD-ROM (with Additional Charge)
    The upgrade service is available in CD-ROM with additional charge.
    For further information, contact your local Renesas Technology sales office or distributor.

    The type name and comment required to order the upgraded product are as follows:
    ComputerOSType NameComment
    IBM PC/AT
    or
    compatible
    Windows 98
    Windows 95
    Windows NT 4.0
    M-PD79SIM For first ordering: W95E
    For upgrading: W95E-VUP-[Serial No.]
    Note: Serial No. need not be entered if you have the license ID.

    2.3 On User's Manual
    The user's manual of the product is included with it in the electronic file (PDF).
    The paperbound version of the manual is also available with additional charge (the contents of it is the same as those in the electronic file). If you need it, please place an order with the following type name and comment filled in:
    Type Name:MESH-TOOL-S
    Comment:PD79SIM-UE




© 2008. Renesas Technology Corp., All rights reserved. Privacy | Legal