|
|
 |
MESC TOOL NEWS:
MESCT-MR30-000901D
MR30 V.3.30 Release 1
Upgraded Version Announcement
|
Real-time OSes MR30 for the M16C/60 and M16C/20 series MCUs have been upgraded as follows:
- Real-time OS development kit: MR30K V.3.30 Release 1
- Real-time OS mass production contract: MR30S V.3.30 Release 1
-
Descriptions of Upgrade
- 1.1 New Features
- (1)The stack calculation utility of NC30WA V.4.00 Release 1 supported.
- (2) The ret_int() system calls inadvertently described in C-written programs interpreted as errors at compilation.
- 1.2 Problems Fixed
- The following known problems have been fixed:
- (1) On modification of the setup file for setting MR30's system timer
- For details refer to "MR30 precaution" issued on February 16, 2000
- (2) On signed 8-bit data types B and VB
- For details refer to "MR308 and MR30 Precautions" issued on May 1, 2000.
- (3) On the prcv_msg system call
- For details refer to "MR30 precaution" issued on June 16, 2000.
-
How to Upgrade Current Products and Order Upgraded Ones
MR30 is a product for a special user.
If you need the latest version of Real-time OS with online, csc@renesas.com.
|
 |