Tool News
 
 
 

Tool News

Products Info
Downloads
Tools FAQs
MESC TOOL NEWS: MESCT-TM_1-000901D

TM V.3.01
Upgraded Version Announcement

This is to announce that integrated development environment TM has been upgraded from its V.2.01 to V.3.01.


  1. Descriptions of Upgrade
    1.1 New Features
    (1) Reconfigured windows in GUI
    Each window separated by function can be opened by the project bar. This allows the user to make efficient use of windows without opening unused ones.
    (2) Read-in of already-existing makefile files
    Creating projects by reading already-existing makefile files enables the user easily to switch from development environment using commands to TM.
    (3) Static analyses of functions and variables
    Absolute object files produced by Build are read in, so that information on the functions and variables contained in these files can be displayed.


    1.2 Compilers on Which TM Runs
    TM V.3.01 can run on the following compilers
    * NC308WA V.3.00 Release 1 or later
    * NC30WA V.4.00 Release 1 or later
    * NC79WA V.4.00 Release 1 or later
    Note: Use TM V.2.01 for any other compilers or versions than shown above. TM V.3.01 can co-reside with TM V.2.01.


  2. How to Upgrade Current Product and Order Upgraded One
    2.1 Online Upgrade (without Charge)
    Please upgrade TM V.3.01 from HERE.
    Notes:
    1. Customers who purchased any of our cross-tool products in CD-ROM on and after September 1 need not upgrade TM since TM V.3.01 is bundled in the CD-ROM.
    2. Customers who have upgraded NC30WA, NC308WA, or NC79WA online are requested to upgrade their TM online.







© 2008. Renesas Technology Corp., All rights reserved. Privacy | Legal