|
|
 |
MESC TOOL NEWS:
MESCT-NC77WA_1-000901D
NC77WA V.5.20 Release 3 Upgraded Version Announcement
|
This is to announce that C compiler NC77WA for the 77xx series MCUs (with an assembler and integrated development environment) has been upgraded from its V.5.20 Release 2 to V.5.20 Release 3.
- Descriptions of Upgrade
- The following known problems have been fixed:
- (1)If two or more sections with the same name are successively defined in a file, an error occurs in LST77 at the definition of the succeeding section.
- For details refer to "LST77 Precaution" issued on April 1, 2000.
- (2)User and group IDs become indefinite at the installation of the product.
- For details refer to "EWS-Version C Compilers Assemblers, and Real-Time OSes Precautions"issued on April 1, 2000.
- (3)Windows' error message may appear when an optimize option used.
- For details refer to "PC-Version NC308WA, NC30WA, NC79WA, NC77WA Precautions" issued on May 1, 2000.
- (4)At typing a command, selecting only an option without specifying the name of a file to convert will force termination of LST77 or LST74.
- For details refer to "LST77 and LST74 Precautions"issued on June 16, 2000.
- (5)Folding floating-point constants may cause incorrect subtract operations to be performed.
- For details refer to "NC308WA, NC30WA, NC79WA, NC77WA Precautions "issued on July 16, 2000.
- (6)Folding constants of type unsigned long may cause incorrect divide and modulus operations to be performed.
- For details refer to "NC308WA, NC30WA, NC79WA, NC77WA Precautions "issued on July 16, 2000.
-
How to Upgrade Current Products and Order Upgraded Ones
- 2.1 Online Upgrade (without Charge)
- Please download the upgraded product from HERE.
- 2.2 First Ordering or Upgrading by CD-ROM (with Additional Charge)
- The upgrade service is available in CD-ROM with additional charge. For further information, contact your local Renesas Technology sales office or distributor.
- The type name and comment required to order the upgraded product are as follows:
| Computer | OS | Type Name | Comment |
IBM PC/AT or compatible | Windows 98 Windows 95 Windows NT 4.0 | M-NC77WA | For first ordering:W95E For upgrading: W95E-VUP-[Serial No.] W95E-GUP-[Serial No.] |
Notes:
1. "GUP" denotes the upgrade from AS77 to NC77WA.
2. Serial No. need not be entered if you have your product's license ID.
|
 |