Tool News
 
 
 

Tool News

Products Info
Downloads
Tools FAQs
MESC TOOL NEWS: MESCT-NC77WA_2-000901D

LST77 and LST74
Upgraded Versions Announcement

This is to announce that absolute address list creating tools LST77 and LST74, which are included with C compiler NC77WA and relocatable assembler RASM 77 for the 77xx series; and relocatable assembler SRA74 for the 740 family of MCUs respectively, have been upgraded as follows:
  • LST77 V.1.00.10
  • LST74 V.1.02.01


  1. Descriptions of Upgrade
    The following known problems have been fixed:
    (1) In LST77, if two or more sections with the same name are successively defined in a file, an error occurs at the definition of the succeeding section.
    For details refer to "LST77 Precaution" issued on April 1, 2000.
    (2)At typing a command, selecting only an option without specifying the name of a file to convert will force termination of LST77 or LST74.
    For details refer to "LST77 and LST74 Precautions" issued on June 16, 2000.


  2. How to Upgrade Current Products and Order Upgraded Ones
    Online Upgrade (without Charge)
    Please download the upgraded product from following tables.

    LST77 V.1.00.10
    ComputerOSSoftwareManual
    IBM PC/AT
    or
    compatible
    Windows 98/95, Windows NT 4.0 lst77.exe (44.0KB) lst77e.pdf (12.7KB)


    LST74 V.1.02.01
    ComputerOSSoftwareManual
    IBM PC/AT
    or
    compatible
    Windows 98/95, Windows NT 4.0 lst74.exe (44.0KB) lst74e.pdf (13.8KB)





© 2008. Renesas Technology Corp., All rights reserved. Privacy | Legal