Tool News
 
 
 

Tool News

Products Info
Downloads
Tools FAQs
MESC TOOL NEWS: MESCT-PD77SIM-000901D

PD77SIM and PD77
Precautions

Please take note of the following problem in using PD77SIM and emulator debugger PD77 for the 77xx series of MCUs:
  • On downloading IEEE-695 absolute format files created by IAR's C compiler ICC7700 (EW7700)


  1. Versions Concerned
    Simulator debugger for the 77xx series: PD77SIM V.3.00 Release 1
    Emulator debugger for the 77xx series: PD77 V.2.00 Release 1 -- V.3.00 Release 1

  2. Problem
    In IEEE-695 absolute format files (hereafter called 695-format files) created by IAR's C compiler ICC7700 (EW7700), the part of programs beyond address 100000h cannot correctly be downloaded.

  3. Condition
    This problem occurs if a 695-format file containing data (including instruction code) beyond address 100000h is downloaded.

  4. Workaround
    The custom window and converter are provided to download 695-format files properly. Please install them into PD77SIM or PD77 in the following procedure:

    (1) Download self-extracting archive "_IARConv.exe" from the following table.
    (2) Decompress the above file on the directory where the executable file of PD77SIM or PD77 is stored; the following files are expanded:
    - IARLoad.p (for the custom window)
    - IARConv.exe (for the converter)
    (3) In PD77SIM or PD77, select [Optional Window] -> [Custom Window] -> [Option] menu. You see the Custom Window Option dialog box.
    (4) Click the Add button in the above dialog box, and IARLoad.p will be registered.

    _IARConv.exe (33.7KB)
    Execute Download


    4.1 How to Use Custom Window
    (1) In PD77SIM or PD77, select [Optional Window] -> [Custom Window]- > [iarload] menu.
    (2) Click the Setup button in the custom window and select executable IARConv.exe for the converter.
    (3) Click the Download button in the custom window and select a 695-format file. Then, the file will be downloaded. Push down the Reload button if re-download necessary.
    Note: When using the custom window, ensure that the script window is open.


  5. Schedule of Fixing Problem
    We plan to fix this problem in our next release.






© 2008. Renesas Technology Corp., All rights reserved. Privacy | Legal