|
|
 |
MESC TOOL NEWS:
MESCT-SRA74-000901D
SRA74 V.4.00 Release 3 Upgraded Version Announcement
|
This is to announce that relocatable assembler SRA74 for the 740 family MCUs has been upgraded from its V.4.00 Release 2 to V.4.00 Release 3.
- Descriptions of Upgrade
- 1.1 Problems Fixed
The following known problems have been fixed:
- (1) When a line with 256 or more characters including a new line
character exists in the symbol file that has not already been
converted by CV74, the file may not be read into the debugger after converted by CV74.
- For details refer to "Precaution Concerning to CV74 Included with SRA74" issued on April 16, 2000.
- (2) User and group IDs become indefinite at the installation of the product.
- For details refer to "EWS-Version C Compilers Assemblers, and Real-Time OSes Precautions" issued on April 1, 2000.
- (3)Invoking programs written in structured description by using the "-ASM" option in LOOP 74 results in errors being generated in SRA74.
- For details refer to "SRA74 for the 740 family of microcomputers " issued on February 16, 1999.
- (4) When labels that are referenced by structured description
instructions described in macro definitions are declared to be those externally referenced,
the declarations made after the lines of macro definitions cannot correctly be dealt with.
- For details refer to "All the versions of SRA74" issued on January 16, 1999.
-
How to Upgrade Current Products and Order Upgraded Ones
- 2.1 Online Upgrade (without Charge)
- Please download the upgraded product from HERE.
- 2.2 First Ordering or Upgrading by CD-ROM (with Additional Charge)
- The upgrade service is available in CD-ROM with additional charge. For further information, contact your local Renesas Technology sales office or distributor.
- (1)The type name and comment required to order the upgraded product are as follows:
| Computer | OS | Type Name | Comment |
IBM PC/AT or compatible | Windows 98 Windows 95 Windows NT 4.0 | M-SRA74 | For first ordering: W95E For upgrading: W95E-VUP-[Serial No.] |
Notes: Serial No. need not be entered if you have your product's license ID.
|
 |