Tool News
 
 
 

Tool News

Products Info
Downloads
Tools FAQs
MESC TOOL NEWS: MESCT-TM_2-000901D

TM
Precaution

Please take note of the following problem in using integrated development environment TM:
  • On reading projects created by TM V.2.xx into TM V.3.xx


  1. Versions Concerned
    TM V.3.00 -- V.3.01

  2. Problem
    When TM V.3.01 reads projects created by TM V.2.xx, some information on the Output directory is lost, which may cause TM not to operate properly.
    2.1 Conditions
    This problem occurs if the following two conditions are satisfied:
    (1) A project has been created by TM V.2.xx in which any of the other directories than the working directory is designated as the Output directory. (For example, ".\Output" is designated as the Output directory.)
    (2) The above project has been read by TM V.3.00 or V.3.01.

  3. Workaround
    This problem can be circumvented by reading projects through the following steps in TM V.2.xx:
    1. Select [Environment]-> [ProjectSettings] menu.
    2. Open the ProjectSettings dialog box and click the TARGET tab.
    3. Enter "." (a period) in edit control "Output Directory".
    4. Execute a build
    5. Read the project after executing a build by TM V.3.00 or V.3.01.

  4. Schedule of Fixing Problem
    We plan to fix this problem in our next release.





© 2008. Renesas Technology Corp., All rights reserved. Privacy | Legal