|
|
 |
MESC TOOL NEWS:
MESCT-M34514T-MCU-000916D
Please take note of the labels on switches SW8 on MCU board M34514T-MCU for the 4513 and 4514 groups in the 4500 MCU series.
- Products Concerned
| Product Type | Description |
M34514T-MCU | MCU board for 4513 and 4514 groups in 4500 series
- Serial Nos. 8FS001 -- 8FS005 fabricated in June 1998 (5 pieces)
- Serial Nos. 8GS006 -- 8GS020 fabricated in July 1998 (15 pieces)
- Serial Nos. 8KS021 -- 8KS040 fabricated in Nov. 1998 (20 pieces)
- Serial Nos. 9AS001 -- 9AS020 fabricated in Jan. 1999 (20 pieces)
- Serial Nos. 9CS021 -- 9CS060 fabricated in Mar. 1999 (40 pieces)
- Serial Nos. 9GS061 -- 9GS090 fabricated in July 1999 (30 pieces)
- Serial Nos. 9JS091 -- 9JS140 fabricated in Oct. 1999 (50 pieces)
|
- Problem
- In some of the M34514T-MCU boards, the following faults of the labels on the SW8 switch will be found:
- (1) No labels are placed on switch SW8.
- (2) The "513" label of SW8 (for the 4513 group) is placed at the position of the "514" label of SW8 (for the 4514 group), and vice versa.
- The positions and settings of switch SW8 on M34514T-MCU
- * Positions

- * Settings

- If M34514T-MCU Used with No Labels:
If these symptoms appear, set the MCU board correctly for the desired MCU group in accordance with M34514T-MCU User's Manual.
- If M34514T-MCU Used with Labels Placed at Opposite Positions:
The 4513 group may be selected for the 4514 group and vice versa. In this case the following symptoms appear:
(1) In the case where "513" (for the 4513 group) is selected by SW8 for the 4514 group
Since the M34514E8FP is mounted on the M34514T-MCU board as the evaluation MCU, programs can be executed properly. However, the MCU file for the 4513 group is automatically selected at launching PD45, so that error messages are displayed when instructions specific to the 4514 group are inputted with assemble commands. Also instructions specific to the 4514 group are not displayed with commands for disassemble displays.
Example: A question mark "?" is displayed as a result of executing a command for program display or real-time trace, for example.
(2) In the case where "514" (for the 4514 group) is selected by SW8 for the 4513 group
Since the MCU specifications of the 4514 group include those of the 4513 group, no problems occur except for the limitations imposed on the M34514T-MCU board. However, the MCU file for the 4514 group is automatically selected at launching PD45, so that error messages are not displayed when instructions specific to the 4514 group are inputted with assemble commands.
|
 |