Tool News
 
 
 

Tool News

Products Info
Downloads
Tools FAQs
MESC TOOL NEWS: MESCT-TM-001016D

TM
Precaution

Please take note of the following problems in using integrated development environment TM:
  • On scanning the dependencies of header files on the source file
  • On adding files to the project
  • On Performing build



  1. Versions Concerned
    TM V.3.00 -- V.3.01 for NC308WA, NC30WA, and NC79WA

  2. Problem on Scanning Dependencies of Header Files on Source File
    2.1 Description
    Even if any header file included in the C source file has already been deleted, scanning the dependencies of header files on the source file by ProjectEditor in TM cannot remove the header file's name concerned from the project.

    2.2 Conditions
    This problem occurs if the following two conditions are satisfied:
    (1) Any header file included in the C source file is deleted or commented out.
    (2) Then, the C source file is scanned by ProjectEditor in TM to update the dependencies of header files on it.

    2.3 Workaround
    Delete files unnecessary for the project by selecting [Project] --> [Delete] menu in ProjectEditor.

    2.4 Schedule of Fixing Problem
    We plan to fix this problem in our next release.


    TM Precaution
    MESCT-TM-001016D

  3. Problem on Adding Files to Project
    3.1 Description
    When adding a file other than a C source file (for example, a header or library file) to the project, the path to the file is fixed in the working directory, resulting in the user-specified path being invalid.

    3.2 Condition
    This problem occurs if any file other than a C source file is added to the project.

    3.3 Workaround
    To add a header file, make an automatic entry by scanning the dependency of it on the source file using ProjectEditor in TM. To add any other file than header files, do once and close the project; then, edit the contents of the project file (with extension ".tmk") by an editor and so on.

    3.4 Schedule of Fixing Problem
    We plan to fix this problem in our next release.


    TM Precaution
    MESCT-TM-001016D

  4. Problem on Performing Build
    4.1 Description
    Even if a compile error arises, build is performed without stopping until linking is complete. However, link errors will be detected because compilation is improperly terminated.

    4.2 Condition
    This problem occurs if any of the assemble command options, for example, -as30, is used as an option for compilation.

    4.3 Workaround
    Should build not stop running even after a compile error arises, cancel the build by selecting [Action] --> [Cancel Build] menu.

    4.4 Schedule of Fixing Problem
    We plan to fix this problem in our next release.






© 2008. Renesas Technology Corp., All rights reserved. Privacy | Legal