Tool News
 
 
 

Tool News

Products Info
Downloads
Tools FAQs
MESC TOOL NEWS: MESCT-M306N0TB-RPD-E-001016D

M306N0TB-RPD-E
Remodeling Announcement

This is to announce that we will remodel emulation pod M306N0TB-RPD-E for the M16C/6N group MCUs to eliminate the problem described below.


  1. Products Concerned
    Product Type: M306N0TB-RPD-E
    Serial Numbers: Those ending with any number or a character of A
    Manufactured in August 1999: 9HS002, 9HS003, 9HS005 -- 9HS007, 9HS009, 9HS011,
    9HS013, 9HS014, 9HS017, 9HS019 -- 9HS022, 9HS025,
    9HS001A, 9HS004A, 9HS008A, 9HS010A, 9HS012A,
    9HS015A, 9HS016A, 9HS018A, 9HS023A, and 9HS024A
    Manufactured in December 1999: 9LS026A -- 9LS046A
    Manufactured in January 2000: 0AS047A -- 0AS063A
    Manufactured in April 2000 0DS066A -- 0DS090A, 0DS092A, 0DS094A, 0DS096A, and
    0DS098A -- 0DS105A


  2. Problem
    If the above pods are used at a frequency of 16 MHz, any of the following symptoms may occur as their internal temperatures rise:
    (1) The program goes into improper operation about ten minutes after turning on the emulator power supply.
    (2) Breaks occur at addresses where no breakpoints have been set.
    (3) An LED turns on, indicating address 00000h has been incorrectly accessed.

    Note: The reproducibility of these symptoms varies with the environment in which the pod is used and the variation between device parameters.

  3. Probable Cause
    The probable cause is that as the internal temperature of the pod rises, the read margin of the emulation memory decreases, resulting in read errors.

  4. Temporary Measure
    Remove the lid at the top of the pod and cool the inside of the pod with the forced circulation of air by fan, for example.

  5. How to Remodel Pods
    The products concerned are remodeled free of charge. Please fill in "M306N0TB-RPD-E Remodeling Application Form" and send your pod to your local Renesas Technology sales office or distributor with the filled-in application form enclosed in it.
    Be aware that we will not be able to supply you with another pod for remodeling period.

    Effective Date of Application: October 16, 2000, to December 21, 2001, inclusive

    Send to: Your local Renesas Technology sales office or distributor





© 2008. Renesas Technology Corp., All rights reserved. Privacy | Legal