Tool News
 
 
 

Tool News

Products Info
Downloads
Tools FAQs
MESC TOOL NEWS: MESCT-TOOL_2-001101D

Information on Mitsubishi Development Support Tools
Running on Windows 2000

This is to inform you which of our tool products are capable of running on Windows 2000.


This news summarizes the results of operations of our software tools tested with a commercial version of Windows 2000 Professional.

  1. Conditions for Running software tools on Windows 2000
    • To install software tools, the user have to be granted the administrator privilege.
    • To run a software tool under normal conditions, the user have to gain a write permission for the directory where the tool has been installed.


  2. Software Tools Running on Windows 2000
    (1)Products for Common Use
    Tool NameCapability of Running on Windows 2000Versions
    TMO.K. Note 1V.2.01 and later (for CC32R, NC77WA, and SRA74)
    V.3.01 and later (for NC308WA, NC30WA, and NC79WA)
    MMO.K.All versions

    (2)Products for M32R Family of 32-Bit MCUs
    Tool NameCapability of Running on Windows 2000Versions
    CC32RO.KAll versions
    MR32RO.K.All versions
    PD32RSIMO.K. Note 2V.1.00 Release 1 and later
    PD32RNG Next version and later capable-
    PD32000NG Not for the present-

    (3)Products for M16C/80 Series of 16-Bit MCUs
    Tool NameCapability of Running on Windows 2000Versions
    NC308WA O.K. All versions
    AS308O.K.All versions
    MR308O.K.All versions
    PD308SIMO.K. Note 2V.2.00 Release 1 and later
    PD308O.K.V.2.10 Release 1 and later

    (4)Products for M16C/60 and M16C/20 Series of 16-Bit MCUs
    Tool NameCapability of Running on Windows 2000Versions
    NC30WA O.K. All versions
    AS30O.K.All versions
    MR30O.K.All versions
    PD30SIMO.K. Note 2V.4.00 Release 1 and later
    PD30O.K.V.5.10 Release 1 and later

    (5)Products for 7900 Series of 16-Bit MCUs
    Tool NameCapability of Running on Windows 2000Versions
    NC79WA O.K. All versions
    AS79O.K.All versions
    MR79O.K.All versions
    PD79SIMO.K. Note 2V.3.10 Release 1 and later
    PD79O.K.V.3.10 Release 1 and later

    (6)Products for 77xx Series of 16-Bit MCUs
    Tool NameCapability of Running on Windows 2000Versions
    NC77WA O.K. V.4.00 Release 1 and later
    RASM77O.K.V.5.00 Release 1 and later
    PD77SIMO.K. Note 2V.3.00 Release 1 and later
    PD77O.K.V.3.10 Release 1 and later
    PDB77NG Not for the present-

    (7)Products for 740 Family of 8-Bit MCUs
    Tool NameCapability of Running on Windows 2000Versions
    SRA74O.K. V.4.00 Release 1 and later
    PD38SIMO.K. Note 2V.2.00 Release 1 and later
    PD38O.K.V.4.10 Release 1 and later

    (8)Products for 4500 and 720 Series of 4-Bit MCUs
    Tool NameCapability of Running on Windows 2000Versions
    PD45O.K.V.1.30 Release 1 and later
    RTT72NG Not for the present-
    RTT72SNG Not for the present-

    Notes 1:
    TM V.2.01 will fail in build or rebuild if either one of the following conditions is met:
    * Build or rebuild is performed for the first time after creating a project.
    * Build is performed while no relocatable or absolute object files exist.
    [Workaround] When "Build" or "Rebuild" fails, please execute "Build" again.
    Notes 2:
    To run these software tools under normal conditions, the user have to gain write permissions for the directories where Windows 2000 and each of the tools have been installed.





© 2008. Renesas Technology Corp., All rights reserved. Privacy | Legal