Tool News
 
 
 

Tool News

Products Info
Downloads
Tools FAQs
MESC TOOL NEWS: MESCT-TM_1-001216D

TM V.3.10
Upgraded Version Announcement

This is to announce that integrated development environment TM has been upgraded from its V.3.01 to V.3.10.


  1. Descriptions of Upgrade
    1.1 New Features
    (1) Supported by CC32R, NC77WA, and SRA74
    TM V.3.10 can run on the following products:
    • NC30WA V.4.00 Release 1 or later
    • NC308WA V.3.00 Release 1 or later
    • NC79WA V.4.00 Release 1 or later
    • CC32R V.3.00 Release 1 or later
    • NC77WA V.5.20 Release 4 or later
    • SRA74 V.4.10 Release 1 or later
    If you are using any of the tool products whose versions are not shown here, use TM V.2.01 instead. TM V.3.10 and TM V.2.01 can co-reside in the same operating environment.
    (2) Views in the Inspector window improved
    Defining and referencing functions and variables and the verbose settings of the inspector can easily be switched by selecting each tab.

    1.2 Problems Fixed
    (1) When TM V.3.xx reads projects created by TM V.2.xx, some information on the Output directory is lost.
    For details refer to MESC TOOL NEWS "TM Precaution" issued on September 1, 2000.

    (2) Even if any header file included in a C source file has been deleted, scanning the dependencies of header files on the source file cannot remove the header file's name concerned from the project.
    For details refer to MESC TOOL NEWS "TM Precaution" issued on October 16, 2000.

    (3) When a file other than a C source file (for example, a header or library file) is added to the project, the path to the file is fixed in the working directory, resulting in the user-specified path being invalid.
    For details refer to MESC TOOL NEWS "TM Precaution" issued on October 16, 2000.

    (4) Adding a new build option or overwriting an existing one by performing a specific procedure may force Windows to be terminated.
    For details refer to MESC TOOL NEWS "TM Precaution" issued on November 16, 2000.


  2. How to Upgrade Current Product
    2.1 Online Upgrade (without Charge)
    Please download the upgraded product from our tool homepage at HERE.

    Notes:
    The customer who has upgraded NC30WA, NC308WA, NC79WA, CC32R, NC77WA, or SRA74 online is also requested to upgrade TM online.







© 2008. Renesas Technology Corp., All rights reserved. Privacy | Legal