|
|
 |
MESC TOOL NEWS:
MESCT-NC79WA-001216D
NC79WA V.4.10 Release 1 Upgraded Version Announcement
|
This is to announce that C compiler NC79WA (with an assembler and integrated development environment) for the 7900 series MCUs has been upgraded from its V.4.00 Release 1 to V.4.10 Release 1.
- Descriptions of Upgrade
- 1.1 New Features
| (1) | Incrementing and decrementing pointer variables of type far and assigning constants to successive areas further optimized |
| (2) | Function-extending #pragma directive TBLJMPOFF introduced (this function warns that the table jump code created using the -fswitch_table[-fST] option spreads across the bank boundary) |
| (3) | Capable of assigning pointer variables using the DPnDATA declaration utility with no option selected |
- 1.2 Problems Fixed
| (1) | Assigning the address of a function to a variable of type pointer to another function results in a System Error being generated if the types of both functions are different from each other.
For details refer to MESC TOOL NEWS "NC308WA, NC30WA, NC79WA, NC77WA Precautions" issued on July 16, 2000. |
| (2) | The total size of ROM displayed on-screen at completion of linking may differ from the one outputted to the MAP file.
For details refer to MESC TOOL NEWS "NC308WA, NC30WA, NC79WA, AS308, AS30, and AS79Precautions" issued on October 1, 2000. |
| (3) | If the condition expression in an if statement comprises two or more expressions testing a bit field each and performs the logical AND operation of them, incorrect code will be generated.
For details refer to MESC TOOL NEWS "NC308WA V.3.00 Release 1, NC30WA V.4.00 Release 1 and NC79WA V.4.00 Release 1 Precautions" issued on October 1, 2000. |
| (4) | When the relative path is applied to operands of assembler directive ".include", include files cannot be found even when a source file hitherto having no problem is assembled.
For details refer to MESC TOOL NEWS "NC308WA, NC30WA, NC79WA, AS308, AS30, and AS79 Precautions" issued on November 1, 2000. |
- How to Upgrade Current Product and Order Upgraded One
- 2.1 Online Upgrade (without Charge)
- Please download the upgraded product from HERE.
- 2.2 First Ordering or Upgrading by CD-ROM (with Additional Charge)
- Upgrade service in CD-ROM is also available with additional charge. For further information, contact your local Renesas Technology sales office or distributor.
- The type name and comment required to order the upgraded product are shown below.
| Computer | OS | Type Name | Comment |
| IBM PC/AT or compatible | Windows 98 Windows 95 Windows 2000 Windows NT 4.0 |
M-NC79WA | For first ordering: W95E For upgrading: W95E-VUP-[Serial No.] |
* Serial No. need not be entered if you have the license ID.
|
 |