|
|
 |
MESC TOOL NEWS:
MESCT-NC77WA-001216D
NC77WA V.5.20 Release 4 Upgraded Version Announcement
|
This is to announce that C compiler NC77WA (with an assembler and integrated development environment) for the 77xx series MCUs has been upgraded from its V.5.20 Release 3 to V.5.20 Release 4.
- Descriptions of Upgrade
- 1.1 New Feature
- TM V.3.10 supported
- 1.2 Problem Fixed
- The known problem described below has been fixed.
- (1) When bit fields are used both in "if" and "else if" statements in an "if - else if" construct, codes may be created which make opposite decisions as to whether the results of evaluating expressions are TRUE or not. For details refer to MESC TOOL NEWS "NC77WA Precaution " issued on November 16, 2000.
- How to Upgrade Current Product and Order Upgraded One
- 2.1 Online Upgrade (without Charge)
- Please download the upgraded product from HERE.
- 2.2 First Ordering or Upgrading by CD-ROM (with Additional Charge)
- Upgrade service in CD-ROM is also available with additional charge. For further information, contact your local Renesas Technology sales office or distributor.
- The type name and comment required to order the upgraded product are
shown below.
| Computer |
OS |
Type Name |
Comment |
| IBM PC/AT or compatible |
Windows 98 Windows 95 Windows 2000 Windows NT 4.0 |
M-NC77WA |
For first ordering: W95E For upgrading: W95E-VUP-[Serial No.]
or: W95E-GUP-[Serial No.] |
| Notes: | 1. "GUP" denotes the upgrade from RASM77 to NC77WA. |
|
| 2. Serial No. need not be entered if you have the license ID. |
|
 |