Tool News
 
 
 

Tool News

Products Info
Downloads
Tools FAQs
MESC TOOL NEWS: MESCT-SRA74-001216D

SRA74 V.4.10 Release 1
Upgraded Version Announcement

This is to announce that relocatable assembler SRA74 for the 740 family MCUs has been upgraded from its V.4.00 Release 3 to V.4.10 Release 1.


  1. Description of Upgrade
    1.1 New Features
    (1) TM V.3.10 supported
    (2) The maximum number of characters specified by pseud instruction .COL changed to 512. This allows a maximum of 512 characters to be displayed in every line of the print file.


  2. How to Upgrade Current Product and Order Upgraded One
    2.1 Online Upgrade (without Charge)
    Please download the upgraded product from HERE.

    2.2 First Ordering or Upgrading by CD-ROM (with Additional Charge)
    Upgrade service in CD-ROM is also available with additional charge. For further information, contact your local Renesas Technology sales office or distributor.

    The type name and comment required to order he upgraded product are shown below.
    Computer OS Type Name Comment
    IBM PC/AT or compatible Windows 98
    Windows 95
    Windows 2000
    Windows NT 4.0
    M-SRA74 For first ordering: W95E
    For upgrading: W95E-VUP-[Serial No.]
    Note: Serial No. need not be entered if you have the license ID.





© 2008. Renesas Technology Corp., All rights reserved. Privacy | Legal