Tool News
 
 
 

Tool News

Products Info
Downloads
Tools FAQs
MESC TOOL NEWS: MESCT-TM_2-001216D

TM
Precaution

Please take note of the problem inscribed below in using integrated development environment TM.
  • On canceling builds


  1. Versions Concerned
    TM V.3.00 -- V.3.10

  2. Problem
    When builds or rebuilds are canceled, the cancellation cannot properly be terminated. So, TM may not continue its operation.

    2.1 Conditions
    This problem occurs if the following two conditions are satisfied:
    (1) The host OS is Windows 2000 or Windows NT.
    (2) A build is canceled before the message indicating the state of the build is displayed on the Builder window after pressing the Build or Rebuild button on TM.

  3. Workaround
    Avoid satisfying the above conditions.
    If the problem occurs, restore Builder to its previous state with the following steps:
    (1) Press CTRL+ALT+DEL to display Windows' Security window.
    (2) Click the Task Manager button and invoke Windows' task manager.
    (3) Click the Process tab.
    (4) Select the following Image Names out of the processes displayed and click the End Process button:
    (a) cmd.exe
    (b) make.exe
    (c) mtmsubp.exe
    Notes:
    * Be sure to close the processes in order of (a), (b) and (c). However, you need not close processes not shown in the Process tab.
    * Check the state of Builder every time a process is closed. When the Cancel button on the Builder window is displayed in shades of gray, it indicates the normal state, so do not close the process.

  4. Schedule of Fixing Problem
    We plan to fix this problem in our next release.




© 2008. Renesas Technology Corp., All rights reserved. Privacy | Legal