Tool News
 
 
 

Tool News

Products Info
Downloads
Tools FAQs
MESC TOOL NEWS: MESCT-TM-010116D

TM
Precaution

Please take note of the following problems in using integrated development environment TM for Mitsubishi microcomputers:
  • On running TM on Windows 2000
  • On using Inspector
  • On operations in the working directory
  • On using function "Open Project" on the project bar


  1. Problem on Running TM on Windows 2000
    1.1 Version Concerned
    TM V.3.10

    1.2 Description
    When any button or menu on the project bar of TM running on Windows 2000 is clicked, the error message shown below may appear, TM getting unstable.
    "xxx.exe has generated errors and will be closed by Windows. You will need to restart the program."

    1.3 Workaround
    The modified file for circumventing this problem is available in 496-KB self-extracting archive. If necessary, please install the modified file into TM V.3.10 through the following steps:
    (1) Download the patch file(496.4-KB) from HERE.
    (2) Decompress the file on the directory where TM V.3.10 exists.

    1.4 Schedule of Fixing Problem
    We plan to fix this problem in our next release.



    TM Precaution
    MESCT-TM-010116D

  2. Problem on Using Inspector
    2.1 Versions Concerned
    TM V.3.00 -- V.3.10

    2.2 Description
    The inspector of the above versions cannot be used for the programs produced by SRA74 and NC77WA (including RASM77). This has been omitted in TM's manual and release note.

    2.3 Schedule of Fixing Problem
    We plan to add this item to the manual and release note in our next release.
    However, we are not going to implement this specification in SRA74 and NC77WA (including RASM77).



    TM Precaution
    MESCT-TM-010116D

  3. Problem on Operating in Working Directory
    3.1 Versions Concerned
    TM V.3.00 -- V.3.10

    3.2 Description
    Internal errors may arise at saving projects or exiting the project editor.

    3.3 Condition
    This problem occurs if a period ( . ) is included in the name of the working directory at creating a project.

    3.4 Workaround
    Don't use any periods in the name of the working directory.

    3.5 Schedule of Fixing Problem
    We plan to fix this problem in our next release.



    TM Precaution
    MESCT-TM-010116D

  4. Problem on Using Function "Open Project" on the Project Bar
    4.1 Version Concerned
    TM V.3.10 (English version only)

    4.2 Description
    When the selection has been changed in the "Files of Type" combo box in the dialog opened by pressing the "Open Project" button on the project bar, the list of the files of the selected type may not be displayed.

    4.3 Condition
    This problem occurs if any type except "ProjectFiles (*.tmk)" is selected in the "Files of Type" combo box.

    4.4 Workaround
    Enter "*.*" as a file name directly into the "File name" list box and press the ENTER key, without changing the selection in the "Files of Type" combo box.

    4.5 Schedule of Fixing Problem
    We plan to fix this problem in our next release.





© 2008. Renesas Technology Corp., All rights reserved. Privacy | Legal