Tool News
 
 
 

Tool News

Products Info
Downloads
Tools FAQs
MESC TOOL NEWS: MESCT-PD32RSIM-010201D

PD32RSIM V.1.10 Release 1
Upgraded Version Announcement

This is to announce that simulator debugger PD32RSIM for the M32R family of MCUs has been upgraded from its V.1.00 Release 1 to V.1.10 Release 1.
  1. Descriptions of Upgrade
    1.1 New Feature
    (1) Supports the function-extending #pragma directives of C compiler CC32R V.3.00 Release 1.
    For details refer to MESC TOOL NEWS "CC32R V.3.00 Release 1 Upgraded Version Announcement" issued on December 16, 2000.

    1.2 Problems Fixed
    The following known problems have been fixed:
    (1) During display of the Source dialog box in the Program or Source window (opened by using the View -> Source button or menu), Windows' error message appears, forcing termination of the program.
    For details refer to MESC TOOL NEWS "PD32RSIM, PD308SIM, PD30SIM, PD79SIM, PD77SIM, PD32000, PD308, PD30, PD79, PD77 Precautions" issued on June 16, 2000.

    (2) If variables in a structure or union the names of whose members contain more than 1024 characters in total are displayed in the C watch, global, file local, and local windows, Windows' error message may appear, causing the program to be terminated forcefully.
    For details refer to MESC TOOL NEWS "PD32RSIM, PD308SIM, PD30SIM, PD79SIM, PD77SIM, PD38SIM, PD32R, PD32000, PD308, PD30, PD79, PD77, PD38, and PD30M Precautions " issued on October 16, 2000.



  2. How to Upgrade Current Product and Order Upgraded One
    2.1 Online Upgrade (without Charge)
    Please download the upgraded product from HERE

    2.2 First Ordering or Upgrading by CD-ROM (with Additional Charge)
    Upgrade service in CD-ROM is also available with additional charge.
    For further information, contact your local Renesas Technology sales office or distributor.

    The type name and comment required to order the upgraded product are shown below.
    ComputerOSType NameComment
    IBM PC/AT or compatible Windows 98
    Windows 95
    Windows 2000
    Windows NT 4.0
    M-PD32RSIM For first ordering: W95E
    For upgrading: W95E-VUP





© 2008. Renesas Technology Corp., All rights reserved. Privacy | Legal