Tool News
 
 
 

Tool News

Products Info
Downloads
Tools FAQs
MESC TOOL NEWS: MESCT-TM-010216D

TM
Precaution

Please take note of the problem described below in using integrated development environment TM.
  • On adding source files


  1. Versions Concerned
    TM V.3.00 -- V.3.10


  2. Problem
    When new source files are added to a project, rebuild cannot properly be executed because no information is fed into "clean", one of the procedures creating object files.


  3. Condition
    This problem occurs if the name of a source file to be added is contained in that of an already-registered source file including its filename extension.

    3.1 Example
    Consider that an already-registered file's name is "abctest.c"; then this problem will occur if the name of a new source file is as follows:
    test.c
    ctest.c or
    bctest.c


  4. Workaround
    Change the name of the source file to be added in order not to meet the above condition.


  5. Schedule of Fixing Problem
    We plan to fix this problem in our next release.





© 2008. Renesas Technology Corp., All rights reserved. Privacy | Legal