|
|
 |
MESC TOOL NEWS:
MESCT-PD32R-010216D
PD32R V.2.00 Release 2 Upgraded Version Announcement
|
This is to announce that emulator debugger PD32R for the M32R family of MCUs has been upgraded from its V.1.00 Release 1 to V.2.00 Release 2.
- Descriptions of Upgrade
- 1.1 New Features
- (1) Capable of customizing the tool bars and shortcut keys
- (2) Shortcut menus available in every window
- (3) Downloads binary data without erasing a symbol information
- (4) Displays the list of labels in the address setting area
- (5) Provides GUI input/output window
- (6) Displays online help in HTML
- (7) Runs on Windows 2000
- (8) Cooperates with cross-tool kit CC32R V.3.00 Release 1 for the M32R family
- (9) Capable of downloading data to external flash ROM areas
- (10) On-the-fly debugging functions improved
- 1.2 Problem Fixed
- The known problem described below has been fixed.
- (1) When a structure or union the names of whose members contain more than 1024 characters in total is displayed in the C watch, global, file local or local window, the program may be forced to terminate.
- For details refer to
MESC TOOL NEWS "PD32RSIM, PD308SIM, PD30SIM, PD79SIM, PD77SIM, PD38SIM, PD32R, PD32000, PD308, PD30, PD79, PD77, PD38, and PD30M Precautions" issued on October 16, 2000.
- How to Upgrade Current Product
- 2.1 Online Upgrade (without Charge)
- Please download the upgraded product from HERE.
- 2.2 Upgrading by CD-ROM (with Additional Charge)
- Upgrade service in CD-ROM is also available with additional charge. For further information, contact your local Renesas Technology sales office or distributor.
- The type name and comment required to order the upgraded product are shown below.
-
| Computer | OS | Type Name | Comment |
IBM PC/AT or compatible |
Windows 98 Windows 95 Windows 2000 Windows NT 4.0 |
M-PD32R |
W95E-VUP |
|
 |