|
|
 |
MESC TOOL NEWS:
MESCT-PD308-010216D
PD308 V.2.10 Release 1 Precaution
|
Please take note of the problem shown below in using emulator debugger PD308 V.2.10 Release 1 for the M16C/80 series of MCUs.
- Version Concerned
PD308 V.2.10 Release 1
- Problem
When using the MR window, the problems shown below are experienced.
- 2.1 Incorrect Display of Contents
- Task names, handler names and contents of mail boxes in the MR window cannot be displayed correctly.
- Condition:
- This problem occurs whenever you use the MR window.
- 2.2 Nothing Displayed
- The MR window may display nothing with error message "Corrupted MR data".
- Condition:
- This problem occurs if either of the following conditions is satisfied:
- (a) In the system definitions of the configuration file, "YES" is selected in Timeout.
- (b) A variable-length memory pool is defined.
- Workaround
Use the MR command in the script window instead of using the MR window.
- Schedule of Fixing Problem
We plan to fix this problem in our next release.
|
 |