Tool News
 
 
 

Tool News

Products Info
Downloads
Tools FAQs
MAEC TOOL NEWS: MAECT-TM_1-010416D

TM V.3.11
Upgraded Version Announcement

This is to announce that integrated development environment TM has been upgraded from V.3.10 to V.3.11.


  1. Descriptions of Upgrade
    (1) Builds can be performed faster.
    (2) The following known problems have been fixed:
    (a) When any button or menu on the project bar of TM running on Window 2000 is clicked, an error message may appear, TM getting unstable.
    (b) If a period ( . ) is included in the name of the working directory at creating a project, internal errors may arise at saving projects or exiting the project editor.
    (c) When the selection has been changed in the "Files of Type" combo box in the dialog opened by pressing the "Open Project" button on the project bar, the list of the files of the selected type may not be displayed.
    For details of (a) -- (c), refer to MESC TOOL NEWS "TM Precaution" issued on January 16, 2001.
    (d) When projects created by TM V.2.00 or V.2.01 are read into TM, errors arise at linking, which prevents builds from being executed properly.
    (e) When the "Scan All Dependencies" menu on the project editor is executed, an error message may appear, forcing the program to be terminated.
    For details of (d) and (e), refer to MESC TOOL NEWS "TM Precaution" issued on February 1, 2001.
    (f) When new source files are added to a project, rebuild cannot properly be executed because no information is fed into "clean", one of the procedures creating object files.
    For details of (f), refer to MESC TOOL NEWS "TM Precaution" issued on February 16, 2001.

  2. Online Upgrade (without Charge)
    Please download the upgraded product from HERE.
    [Notes:]
    (1) The customer who purchased any of our cross-tool products in CD-ROM on and after this April 16 need not upgrade their TM because TM V.3.11 is bundled with the product.
    (2) The customer who has upgraded CC32R, NC308WA, NC30WA, NC79WA, NC77WA, or SRA74 online is requested to upgrade TM online.






© 2008. Renesas Technology Corp., All rights reserved. Privacy | Legal