Tool News
 
 
 

Tool News

Products Info
Downloads
Tools FAQs
MAEC TOOL NEWS: MAECT-PC4701U-010416D

New Emulator PC4701U Announcement

New emulator PC4701U for Mitsubishi's 8- and 16-bit MCUs has been released.


  1. Features
    PC4701U is a new emulator made by combining the advantages of the predecessors, PC4701M and PC4701HS, and is provided with a USB interface. Like the predecessors, it can also be used for either 8- or 16-bit MCUs by replacing emulator MCUs. Its features are as follows:
    (1) Debugging functions and performances are the same as those of PC4701M and PC4701HS.
    (2) As communication interfaces, LPT parallel, USB, and LAN are provided.
    (3) The licenses of the supporting emulator debuggers are bundled.
    (4) Compact design with built-in power supply
    (5) Compliant with overseas standards

    For details of specifications, see the data sheet from HERE.



  2. Ordering Information
    Product TypeType NameComment
    PC4701U PC4701U -



  3. Related Information
    3.1 Production of Old Products
    Since PC4701U has been put on the market, the predecessors, PC4701M and PC4701HS, are stocked only for spare and repair parts, as in the case of PC4701L, PC4700H, and PC4700L.





© 2008. Renesas Technology Corp., All rights reserved. Privacy | Legal