Tool News
 
 
 

Tool News

Products Info
Downloads
Tools FAQs
MAEC TOOL NEWS: MAECT-PD32R-010416D

PD32R
Precaution

Please take note of the following problem in using emulator debugger PD32R for the M32R family of microcomputers:
  • On downloading target programs to external flash memory by using FDD (flash device definition) files included with PD32R


  1. Versions Concerned
    PD32R V.2.00 Release 1 -- V.2.00 Release 2


  2. Description
    When the target program is downloaded to external flash memory by using a specific FDD file, only half of the memory space are available.


  3. Conditions
    This problem occurs if either of the following two FDD files is selected:
    1. MBM29DL32XTE.FDD included with PD32R V.2.00
    2. MBM29DL32XBE.FDD included with PD32R V.2.00


  4. Workaround
    Use the modified MBM29DL32XTE.FDD or MBM29DL32XBE.FDD file.
    They can be downloaded from following:
    MBM29DL32XTE.zip (compressed file 1KB)
    MBM29DL32XBE.zip (compressed file 1KB)


  5. Schedule of Fixing the Problem
    We plan to fix this problem in our next release.





© 2008. Renesas Technology Corp., All rights reserved. Privacy | Legal