|
|
 |
MAEC TOOL NEWS:
MAECT-TM-010516D
Please take note of the following problems in using integrated development environment TM:
- On scanning the dependencies of header files on a source file
- On setting projectbar appearance to AutoHide
- Problem on Scanning the Dependencies of Header Files on a Source File
- 1.1 Version Concerned
- TM V.3.11
- 1.2 Description
- After the dependencies of header files on a source file are scanned, information on the paths of the newly included header files may become incorrect. As these header files cannot be recognized properly, build will be performed unsuccessfully.
- 1.3 Conditions
- If the following three conditions are satisfied, information on the path of header file B described in condition (2) below becomes incorrect:
- (1) In a C source file exists a #include statement where the relative path of header file A is described.
- (2) Header file A in (1) above contains another #include directive that specifies another header file, B.
- (3) The "Scan All Dependencies" menu on the project editor was executed.
- 1.4 Workaround
- Select compiler option "-I" in the Option dialog box, designating the path of the header file concerned as its parameter; then, scan the dependencies again.
- 1.5 Schedule of Fixing the Problem
- We plan to fix this problem in our next release.
- Problem on Setting Projectbar Appearance to AutoHide
- 2.1 Versions Concerned
- TM V.3.10 -- V.3.11
- 2.2 Description
- The projectbar, when its appearance is set to AutoHide to get it out of your way, may not be restored after the operations described in the following conditions section are performed.
- 2.3 Conditions
- This problem occurs if either of the following operations is performed with projectbar appearance being set to AutoHide:
- The ToolsInformation dialog box was closed.
- The Cancel button was pressed in the Customize dialog box.
- 2.4 Workaround
- This problem will be circumvented by using either of the following ways:
(1) Uncheck the AutoHide check box.
(2) Open the Customize dialog box using the [Change Button Position] menu in the projectbar; then click the OK button.
- 2.5 Schedule of Fixing the Problem
- We plan to fix this problem in our next release.
|
 |