Please take note of the following problem in using simulator debugger PD38SIM for the 740 family of microcomputers:
On the help file
Version Concerned
PD38SIM V.2.00 Release 1
Description
The help file included with the product cannot be displayed.
Workaround
Please download the revised version of the help file (PD38SIM.HLP).
Then substitute the downloaded help file for the one in the directory where PD38SIM has been installed.
Revised Version of the Help File: p38shelp.exe (compressed file 109KB)
Schedule of Fixing the Problem
We plan to fix this problem in our next release.