|
|
 |
MAEC TOOL NEWS:
MAECT-PD308-010516D
PD308 V.3.00 Release 1, PD30 V.6.00 Release 1 and PD79 V.4.00 Release 1 Precautions
|
Please take note of the following problem in using emulator debuggers PD308, PD30, and PD79 for Mitsubishi microcomputers:
- On opening source files in the Program and Source windows
- Versions Concerned
| M16C/80 series MCUs | : PD308 V.3.00 Release 1 |
| M16C/60 and /20 series MCUs | : PD30 V.6.00 Release 1 |
| 7900 series MCUs | : PD79 V.4.00 Release 1 |
- Description
The following symptoms may appear in the Program and Source windows:
- The symbol " - " does not appear in the BRK field, so that breakpoints cannot be set.
- The MIX and DIS modes cannot be switched from the SRC mode.
- 2.1 Condition
- When you open files using the Select Source File dialog displayed by selecting the [Option] -> [View] -> [Source...] menu, this problem may occur if files are opened without selecting functions out of the "Func" list box.
- Workaround
When opening files using the Select Source File dialog box, make sure to select functions out of the "Func" list box, as well as selecting function names out of the Object/Source list box.
- Schedule of Fixing the Problem
We plan to fix this problem in our next release.
|
 |