Tool News
 
 
 

Tool News

Products Info
Downloads
Tools FAQs
MAEC TOOL NEWS: MAECT-MM_1-010616D

MM V.3.00 Release 1
Upgraded Version Announcement

Mitsubishi Maskfile converter MM for Mitsubishi's microcomputers has been upgraded from its Version 2.00.20 to Version 3.00 Release 1.


  1. Descriptions of Upgrade
    (1) GUI supported
    GUI allows you to control software more easily than typing commands on the command line.
    Also error-checking function of input data has been improved.
    (2) Function capable of extracting hexadecimal data written in Intel's HEX format added
    Hexadecimal data written in the Intel HEX or expanded Intel HEX format can be extracted from mask files, as well as in Motorola's S format.
    (3) More than one end record in the Intel HEX format admitted
    When two or more end records are contained in data files written in Intel's HEX format, MM has previously treated them as errors.
    Now, upgraded MM V.3.00 Release 1 displays a dialog box conveying an warning message in such a case, and choosing "Yes" in the dialog box allows you to create mask files.
    For details refer to MAEC TOOL NEWS "MM (Maskfile Converter) Precaution " issued on January 16, 2001.


  2. Online Upgrade (Without Charge)
    Please download the upgraded product from HERE.




© 2008. Renesas Technology Corp., All rights reserved. Privacy | Legal