Tool News
 
 
 

Tool News

Products Info
Downloads
Tools FAQs
MAEC TOOL NEWS: MAECT-PD38-010716D

PD38
Precaution

Please take note of the following problem in using emulator debugger PD38 for the 740 family of microcomputers.
  • PD38 cannot be set up when used in combination with emulation pod M37207T-RPD for the 7200 series MCUs


  1. Versions Concerned
    PD38 V.3.00 Release 1A -- V.5.00 Release 1


  2. Description
    When PD38 is used in combination with emulation pod M37207T-RPD, clicking the OK button in the Init dialog box opened at starting PD38 does not allow further set-up with an error message being displayed.


  3. Workaround
    Press the RESET switch three seconds or more after turning on the power supply to the emulator. Then, launch PD38.


  4. Schedule of Fixing the Problem
    We plan to fix this problem in our next release.





© 2008. Renesas Technology Corp., All rights reserved. Privacy | Legal