Tool News
 
 
 

Tool News

Products Info
Downloads
Tools FAQs
MAEC TOOL NEWS: MAECT-PD308SIM-010801D

PD308SIM V.3.00 Release 1
Precaution

Please take note of the following problem in using simulator debugger PD308SIM V.3.00 Release 1 for the M32C/80 and M16C/80 series MCUs.
  • On using instruction BTST


  1. Description
    When the BTST (bit test) instruction is used in S format, the Z and C flags will be set to the incorrect values.

    1.1 Example
    In the program shown below, the Z flag is set to "1" and the C flag to "0" after execution of the BTST instruction while the correct values of the Z and the C flag is "0" and "1" respectively.
    -----------------------------------------------------------------
     MOV.B  #02H,0800H
     MOV.B  #00H,0801H
     BTST:S 1,0800H
    -----------------------------------------------------------------

  2. Workaround
    Please download modified simulator engine SIM308.EXE (self-extracting archive: 110KB).
    Then, replace the current SIM308.EXE file saved in the directory where PD308SIM has been installed with the downloaded one.


  3. Schedule of Fixing the Problem
    We plan to fix this problem in our next release.




© 2008. Renesas Technology Corp., All rights reserved. Privacy | Legal