|
|
 |
MAEC TOOL NEWS:
MAECT-CC32R-010816D
Please take note of the following problems in using cross-tool kit CC32R for the M32R family MCUs:
- On optimization at accessing a volatile area two or more times successively
- On optimization at using uninitialized pointers
- Versions Concerned
CC32R V.1.00 Release 1 -- V.3.00 Release 1
- Problem on Accessing a "volatile" Area Two or More Times Successively
- 2.1 Description
- If a volatile area is accessed two or more times successively by using the same offset operation, optimization covering the -04 option makes the volatile attribute ineffective.
- 2.2 Conditions
- This problem occurs if the following four conditions are satisfied:
- (1) An optimizing option covering -O4 is used (that is, any of the following options is used; -O4, -O5, -O6, -O7, -Otime only and -Ospace only).
- (2) Any of the following variables is declared to be volatile (excluding bit fields):
- (a) a member of a structure or union
- (b) a member of an array
- (c) a portion represented by a pointer plus offset value
- (3) An area including a variable in (2) above is accessed two or more times successively.
- (4) During the successive accesses in (3) above, no function call or no indirect assignment using pointers is performed.
- 2.3 Examples
[Example 1: Source file "sample1.c"]
--------------------------------------------------------------------
extern volatile unsigned short v_array[]; /* Condition 2-(b) */
void foo(void)
{
while (v_array[7] & 4); /* Condition 3 */
/* Condition 4 */
while (!(v_array[7] & 4)); /* Condition 3 */
}
--------------------------------------------------------------------
[Example 2: Source file "sample2.c"]
--------------------------------------------------------------------
extern volatile struct { /* Condition 2-(a) */
int a;
int b;
} v_strarea;
void foo(void)
{
while (v_strarea.a & 4); /* Condition 3 */
/* Condition 4 */
while (!(v_strarea.a & 4)); /* Condition 3 */
}
--------------------------------------------------------------------
[Example 3: Source file "sample3.c"]
--------------------------------------------------------------------
extern volatile long *v_ptr; /* Condition 2-(c) */
int foo(void)
{
int answer;
answer = (*(v_ptr + 7) & 4); /* Condition 3 */
/* Condition 4 */
answer *= (*(v_ptr + 7) & 8); /* Condition 3 */
return answer;
}
--------------------------------------------------------------------
[Examples of typing commands in CC32R (a % sign denotes a prompt)]
--------------------------------------------------------------------
% cc32R -c -O4 sample1.c
% cc32R -c -O4 sample2.c
% cc32R -c -O4 sample3.c
--------------------------------------------------------------------
- 2.4 Workaround
- This problem will be circumvented in any of the following ways:
- (1) Suppress optimization in the -O4 level.
- Optimization covering the -O4 option is performed when optimizing option -O4, -O5, -O6, -O7, -Otime only or -Ospace only has been selected. If you want to use -Otime or -Ospace, select any of those options, -O3, -O2, -O1, and -O0, at the same time.
- (2) Access the volatile area by using a pointer of type volatile.
[Example 1 (modified): Source file "sample1.c"]
-----------------------------------------------------------------
extern volatile unsigned short v_array[];
void foo(void)
{
volatile unsigned short *ptr = &v_array[7];
while (*ptr & 4);
while (!(*ptr & 4));
}
-----------------------------------------------------------------
[Example 2 (modified): Source file "sample2.c"]
-----------------------------------------------------------------
extern volatile struct s_tag {
int a;
int b;
} v_strarea;
void foo(void)
{
volatile int *ptr = &v_strarea.a;
while (*ptr & 4);
while (!(*ptr & 4));
}
-----------------------------------------------------------------
[Example 3 (modified): Source file "sample3.c"
-----------------------------------------------------------------
extern volatile long *v_ptr;
int foo(void)
{
int answer;
volatile long *ptr = v_ptr + 7;
answer = (*ptr & 4);
answer *= (*ptr & 8);
return answer;
}
-----------------------------------------------------------------
- (3) Replace the volatile area with an equivalent bit field.
[Example 1 (modified): Source file "sample1.c"]
-----------------------------------------------------------------
extern volatile struct {
unsigned short u16:16;
} v_array[];
void foo(void)
{
while (v_array[7].u16 & 4);
while (!(v_array[7].u16 & 4));
}
-----------------------------------------------------------------
CC32R Precaution MAECT-CC32R-010816D
- Problem on Using Uninitialized Pointers
- 3.1 Description
- When optimization covering the -O4 option is performed for a program in which uninitialized pointers are used, the compiler may fall into an endless loop and not be able to terminate compilation.
- 3.2 Conditions
- This problem occurs if the following six conditions are satisfied:
- (1) An optimizing option covering -O4 is used (that is, any of the following options is used; -O4, -O5, -O6, -O7, -Otime only and -Ospace only).
- (2) There exist pointers A and B, which are auto variables.
- (3) There exists a loop statement, and before it is placed either of the following statements:
- (a) an "if" statement, where if the result of the evaluation of the conditional expression is TRUE, an assignment is made to A; if FALSE, no assignment is made.
- (b) a "for" or "while" statement, which contains an assignment expression to A.
- (4) An "if-else" construct is included in the loop in (3), and the value of pointer A is assigned to pointer B in the program statement of "else".
- (5) Until pointer A is referenced in (4), there exists no assignment expression to pointer A except the one in (3)-(a) or -(b).
- (6) There exists no assignment expression to pointer B except the one in (4).
- 3.3 Examples
[Example 1: Source file "sample1.c"]
--------------------------------------------------------------------
int check1, check2;
void
func(void)
{
int *ptr_A; /* Pointer A */ /* Condition 2 */
int *ptr_B; /* Pointer B */ /* Condition 2 */
int i;
if (check1) { /* Condition 3-(a) */
ptr_A = 0; /* Condition 3-(a) */
} /* Condition 3-(a) */
for (i = 0; i < 20; i++) {
if (check2) {
} else {
ptr_B = ptr_A; /* Conditions 4, 5 */
}
}
}
--------------------------------------------------------------------
[Example 2: Source file "sample2.c"]
--------------------------------------------------------------------
int check1, check2;
void
func(void)
{
int *ptr_A; /* Pointer A */ /* Condition 2 */
int **ptr_B; /* Pointer B */ /* Condition 2 */
int i;
while (check1) {
ptr_A = 0; /* Condition 3-(b) */
}
:
for (i = 0; i < 20; i++) {
if (check2) {
:
} else {
ptr_B = (int**)*ptr_A; /* Conditions 4, 5 */
}
}
}
--------------------------------------------------------------------
[Examples of typing commands in CC32R (a % sign denotes a prompt)]
--------------------------------------------------------------------
% cc32R -c -O4 sample1.c
% cc32R -c -O4 sample2.c
--------------------------------------------------------------------
- 3.4 Workaround
- This problem will be circumvented in either of the following ways:
- (1) Suppress optimization in the -O4 level.
- Optimization covering the -O4 option is performed when optimizing option -O4, -O5, -O6, -O7, -Otime only or -Ospace only has been selected. If you want to use -Otime or -Ospace, select any of those options, -O3, -O2, -O1, and -O0, at the same time.
- (2) Initialize pointer A
- Add a code that is sure to initialize pointer A according to the example shown below.
[Example 1 (modified): Source file "sample1.c"]
---------------------------------------------------------------
int *ptr_A;
|
int *ptr_A = 0;
---------------------------------------------------------------
Modify Example 2 above by initializing pointer A in the same way.
|
 |