|
|
 |
MAEC TOOL NEWS:
MAECT-M32100T2-SDI-E-010901D
New Product M32100T2-SDI-E Announcement
|
This is to announce the issuance of new emulator M32100T2-SDI-E for the 32102/32121/3217x group of the M32R/E series MCUs
- Features
- M32100T2-SDI-E is provided with the functions entirely identical to current M32100T-SDI-E plus a USB interface, and its features are as follows:
- (1) Provided with the same debugging functionality and performance as M32100T-SDI-E
- (2) Outfitted with a USB, an LPT parallel, and a LAN communication interface
- (3) Bundled with emulator debugger PD32R
Be sure to use PD32R V.2.10 Release 1 or later as an emulator debugger. It can be downloaded online without charge from HERE.
- (4) Compliant to overseas standards
- To view detailed specifications of the product, go to the data sheet.
- Ordering Information
| Product Type | Type Name | Comment |
| M32100T2-SDI-E |
M32100T2-SDI-E |
- |
- Production of the Old Product
Since M32100T2-SDI-E has been put on the market, the predecessor, M32100T-SDI-E, is stocked only for spare and repair parts.
|
 |