|
|
 |
MAEC TOOL NEWS:
MAECT-PD45-010901D
PD45 V.1.31 Release 1 Upgraded Version Announcement
|
This is to announce that emulator debugger (with an assembler) PD45 for the 4500 series MCUs has been upgraded from V.1.30 Release 1 to V.1.31 Release 1.
- Descriptions of Upgrade
- 1.1 New Features
- (1) The MCU data files for the following MCUs added
- M34524M8, M34524MC, and M34524ED
- M34554M8, M34554MC, and M34554ED
Those for the following MCUs were already introduced on MAEC TOOL NEWS "Announcement of New MCUs Supported by PD45" issued on September 1, 2000.
- M34506M2 and M34506M4
- M34507M2 and M34507M4
(2) Capable of running on Windows 2000
- 1.2 Problem Fixed
- A newly-found problem described below has been fixed.
Problem: When a target program is executed by using any of the following commands and key, PD45 does not stop its display even when execution halted:
- Go command
- GoBreak command
- F1 key
- How to Upgrade Current Product and Order Upgraded One
- 2.1 Online Upgrade (without Charge)
- Please download the upgraded product from HERE.
- 2.2 First Ordering or Upgrading by CD-ROM (with Additional Charge)
- Upgrade service in CD-ROM is also available with additional charge.
For further information, contact your local Renesas Technology sales office or distributor.
- [First Ordering]
| Product Type: | PD45 |
| Version No.: | V.1.31 |
| Release No.: | Release 1 |
| Language: | English |
| ------------------------- |
| Host OS: |
Windows Me, Windows 98, Windows 95, Windows 2000, or Windows NT 4.0 |
- [Upgrading by CD-ROM]
- Please let us know your product's license ID or serial number besides the above information.
|
 |