Tool News
 
 
 

Tool News

Products Info
Downloads
Tools FAQs
MAEC TOOL NEWS: MAECT-TM-011016D

TM
Precaution

Please take note of the following problem in using integrated development environment TM.
  • On setting library paths in compiler M3T-CC32R for the M32R family MCUs


  1. Versions Concerned
    TM V.3.00 -- V.3.11 supported by M3T-CC32R V.2.00 Release 1 -- V.3.10 Release 1


  2. Description
    When TM is working in combination with M3T-CC32R, if options "-L" and "-l" (for selecting a search directory for a library and selecting a library file respectively) of the lnk32r linker are selected on TM's option browser, lnk32r cannot search for the library file at a build, which causes an error to appear.


  3. Workaround
    Edit an internal file used by TM as follows:
    (1) Back up the file to edit; then close TM.
    (2) Open the file "lnk32r.opt" by using the editor. This file is found in directory \mtool\lib32r (the directory where M3T-CC32R has been installed).
    (3) Cut lines 17 through 22 of the file and paste this block to line 31 (immediately before [-LOC]).
    [Block to Cut]
    -----------------------------------------------------------
      [-l]
           TYPE="LNKLIB"
           JPN="....."
           ENG="Specifies a library named lib."
           PARAM="MST"
           SPACE="USE"
    -----------------------------------------------------------
    (4) Save the file.


  4. Schedule of Fixing the Problem
    We plan to fix this problem in our next release.





© 2008. Renesas Technology Corp., All rights reserved. Privacy | Legal