|
|
 |
MAEC TOOL NEWS:
MAECT-M3T-PD45-011016D
Please take note of the following problem in using emulator debugger (with an assembler) M3T-PD45 for the 4500 series MCUs.
- On using the optimizing function of a branch instruction in assembler ASM45
- Versions Concerned
M3T-PD45 V.1.10 Release 1 -- V.1.31 Release 1
- Description
ASM45 may fail to optimize the description that contains a branch-optimizing instruction "BRN" and result in an out-of-range error.
- 2.1 Conditions
- This problem may occur if the following two conditions are satisfied:
- (1) The label used as the operand of a "BRN" instruction is forward referencing.
- (2) The label in (1) above is described in the next page to the one where the "BRN" instruction has been described.
Note that the problem will not arise when the operand of the "BRN" instruction is either an immediate address or a backward-referencing label.
- 2.2 Example
------------------------------------------------------------------
.org 0h,7bh
BRN lab1 ; <-- Processed as a "B" instruction, resulting
in an error
BRN lab2
BRN lab3
lab1: nop ; A forward-referencing label
lab2: nop
lab3:
------------------------------------------------------------------
- Workaround
Change the "BRN" instruction in the line where an error will appear to the "BL" instruction (jump to an address out of the page).
- Schedule of Fixing the Problem
We plan to fix this problem in our next release.
|
 |