Tool News
 
 
 

Tool News

Products Info
Downloads
Tools FAQs
MAEC TOOL NEWS: MAECT-M3T-SRA74-011201D

M3T-SRA74
Precaution

Please take note of the following problems in using relocatable assembler M3T-SRA74 for the 740 family MCUs:
  • On the total number of characters of a line in source files processed by sra74
  • On symbol file conversions in cv74


  1. Problem on the Total Number of Characters of a Line in Source Files Processed by sra74
    1.1 Product and Version Concerned
    Structured relocatable macro assembler sra74 V.4.10.00 included in relocatable assembler M3T-SRA74 V.4.10 Release 1 for the 740 family MCUs

    1.2 Description
    If the total number of characters of any line in a source file exceeds 255 (except for comment lines), the line may not correctly be assembled, and an error will arise in sra74 or link74.

    1.3 Workaround
    Limit the total number of characters of a line to 255 (except for comment lines).

  2. Problem on Symbol File Conversions in cv74
    2.1 Product and Version Concerned
    File conversion tool cv74 V.1.00.01 for the M37280 MCU included in relocatable assembler M3T-SRA74 V.4.00 Release 3 through V.4.10 Release 1 for the 740 family MCUs

    2.2 Description
    If any global bit symbol exists in a symbol file, cv74 fails to convert the file to the one that can be handled by debuggers, resulting in the following error message being displayed.
    Error: Symbol file line characters exceed
    2.3 Workaround
    When making a file conversion by cv74, place a new-line code immediately after the last character of the final line in the symbol file in advance.




© 2008. Renesas Technology Corp., All rights reserved. Privacy | Legal