Tool News
 
 
 

Tool News

Products Info
Downloads
Tools FAQs
MAEC TOOL NEWS: MAECT-MM-020201D

Maskfile Converter MM
Upgraded to V.3.00 Release 2

We have upgraded Mitsubishi Maskfile converter MM from V.3.00 Release 1 to V.3.00 Release 2.


  1. Descriptions of Upgrade
    1.1 Functions Improved
    (1) Checking function of input data has been more improved.
    (2) Explanations and messages displayed on windows have been modified to make the operation of MM easier.

    1.2 Problems Fixed
    The following known problems have been fixed:
    (1) On filename extensions of OSD font data files (.hfd, for example) and
    (2) On making mask files by using the Create Mask File wizard
    For details, see MAEC TOOL NEWS "MM V.3.00 Release 1 Precaution" issued on August 1, 2001.
    (3) On creating mask files with hexadecimal data files treated by MM being saved in the root directory
    For details, see MAEC TOOL NEWS "MM V.3.00 Release 1 Precaution" issued on August 16, 2001.

  2. How to Upgrade the Current Product
    Online Upgrade (without Charge)
    Please download the upgraded product from HERE.




© 2008. Renesas Technology Corp., All rights reserved. Privacy | Legal