Tool News
 
 
 

Tool News

Products Info
Downloads
Tools FAQs
MAEC TOOL NEWS: MAECT-PC7501-020501D

New Emulator PC7501

New emulator PC7501 for the M16C family MCUs has been released. It can operate at frequencies over 20 MHz.


  1. Features
    PC7501 is a full-bus-trace emulator for the M16C family MCUs and especially aims to support MCUs operating at 66 MHz. It allows you to configure the emulator system for every target MCU of the family in combination with the M3xxxxTx-EPB emulation probe and the M3T-PD308F emulator debugger for the M32C/80 Series MCUs.
    For information about M3xxxxTx-EPB and M3T-PD308F, see the succeeding item of news, New Emulation Probe M30830T-EPB and New Emulator Debugger M3T-PD308F V.1.00 Release 1.

    PC7501 provides much more enhanced debugging functions than the current product, PC4701U. It also supplies substantially space-saved debugging environment by its compact design and flexibility of meeting the future evolution of MCUs.

    It has been qualified for the required overseas standards (FCC Rules and CE Marking), so it can be used worldwide.

    For further information, please go to the data sheet.


  2. Ordering Information
    When you place an order of PC7501, please contact your local Renesas Technology sales office or distributor.
    Product TypeType NameComment
    PC7501PC7501-




© 2008. Renesas Technology Corp., All rights reserved. Privacy | Legal