Tool News
 
 
 

Tool News

Products Info
Downloads
Tools FAQs
MAEC TOOL NEWS: MAECT-TM-020516D

A Note on Integrated Development Environment
TM V.3.11

Please take note of the following problem in using integrated development environment TM V.3.11:
  • On deleting source files from a project


  1. Description
    Even when any source file is deleted from a project, information concerning the deleted file may not automatically be erased from the command file for linking (.cmd). Then, TM tries to link the deleted source file at a build, resulting in a link error.

  2. Condition
    This problem occurs if "740 Family" (for SRA74) is selected as the target at creating a project.

  3. Workaround
    After deleting a source file from a project, edit the command file for linking (.cmd) through the following procedures:
    (1) Open the project editor.
    (2) Select ".\project name.cmd" on the project tree.
    (3) Click [Project] -> [Edit Item] -> [Command] menu to open the command dialog box.
    (4) Select the name of the deleted file from the list and click the Delete button.
    (5) Click the OK button.

  4. Schedule of Fixing the Program
    We plan to fix this problem in our next release.




© 2008. Renesas Technology Corp., All rights reserved. Privacy | Legal