Tool News
 
 
 

Tool News

Products Info
Downloads
Tools FAQs
MAEC TOOL NEWS: MAECT-M3T-PD32R-020701D

Emulator Debugger M3T-PD32R
Upgraded to V.3.00 Release 1

Emulator debugger M3T-PD32R for the M32R family MCUs has been upgraded from V.2.10 Release 1 to V.3.00 Release 1.


  1. Descriptions of Upgrade
    1.1 Functions Improved
    (1)Capable of running on Windows XP
    (2)Setting hardware breakpoints and trace events
    (3)Editing source files on the Source and Program windows
    (4) Automatically updating the addresses displayed on the Memory window according to the position of the stack pointer
    (5)Saving MIX displays on the Source and Program windows in files
    (6)Dragging and dropping the reads of files, event settings, and so on
    (7)Renewal of the design of the toolbar's buttons

    1.2 Problems Fixed
    The following known problems have been fixed:
    (1) On turning on the power supply to the target MCU after turning it off
    For details, see MAEC TOOL NEWS "A Note on Emulators M32100T2-SDI-E, M32100T-SDI-E, and M32170T-SDI" issued on March 1, 2002.
    (2) On downloading target programs
    (If a Windows application is launched or any of the other already-opened Windows applications is made active while you are downloading a target program (a load module), the debugger may freeze suddenly.)
    (3)On opening the Source window
    (The Source window may not be opened or not display materials normally if opened.)
    For details of (2) and (3), see MAEC TOOL NEWS "M3T-PD32RSIM, M3T-PD308SIM, M3T-PD30SIM, M3T-PD79SIM, M3T-PD77SIM, M3T-PD38SIM, M3T-PD32R, M3T-PD308, M3T-PD30, M3T-PD79, M3T-PD77, M3T-PD38, PD308M, and PD30M Precautions" issued on December 16, 2001.

  2. How to Upgrade Current Product and Order Upgraded One
    2.1 Online Upgrade (without Charge)
    Please download the upgraded product from HERE.

    2.2 Upgrade in CD-ROM (with Additional Charge)
    Upgrade service in CD-ROM is also available. When you place an order, please furnish the following information to your local Renesas Technology sales office or distributor:

    Product Type:M3T-PD32R
    Version number:V.3.00
    Release number:Release 1
    -------------------------
    Language:English
    -------------------------
    Host OS: Windows XP, Windows Me, Windows 98, Windows 95, Windows 2000, or Windows NT 4.0




© 2008. Renesas Technology Corp., All rights reserved. Privacy | Legal