Tool News
 
 
 

Tool News

Products Info
Downloads
Tools FAQs
MAEC TOOL NEWS: MAECT-M30830T-EPB-020701D

Free-of-Charge Upgrade of MCU
on Emulation Probe M30830T-EPB
(Specific Product)

We replace your MCU on emulation probe M30830T-EPB (specific product) with the upgraded one free of charge. M30830T-EPB is used for emulator PC7501 for the M32C/81, M32C/82, and M32C/83 group MCUs.


  1. Emulation Probes Concerned
    Product TypeSerial Numbers
    M30830T-EPB 1JI001--1JI050

    Total of 50 probes
    Serial numbers have been inscribed on each MCU-mounting board (M30830T-EPBM).
    Note that the products whose serial number ends with "A" already have the upgraded MCUs on them, so they need not be upgraded.

  2. Description of Upgrade
    We replace your MCU mounted on the probe with the upgraded one.
    This upgrade will eliminate the following limitations imposed on the MCU:
    (1) Using the mov instruction to rewrite the function select register C (address 03AFh). This register cannot be read out.
    (2) Setting SFR for CAN after disabling interrupts when CAN functions used. Or setting the levels of the interrupts that may be generated to any of 7, 3, and 1 if you are not allowed to disable interrupts.
    (3) Using timer B in Timer or Event Counter mode when used. If the timer is used in Pulse Width or Pulse Period Measurement mode, no interrupts might be generated depending on the input timing of pulses from the Tbjin pin.
    (4) When the intelligent I/O is used for reception in serial I/O mode synchronized with the internal clock, stopping the clock under software control as soon as the reception has been completed.
    (5) When the intelligent I/O synchronized with the internal clock is used for reception, permitting reception 1 clock after the base timer has been started.

  3. How to Upgrade
    (1) First, fill in the "Free-of-Charge M30830T-EPB (Specific Product) Upgrade Application Form" and send it by e-mail to your local Renesas Technology sales office or distributor.
    (2) Then, send your M30830T-EPB product to them, with the filled-in application form enclosed in it.
    (3) We will ship back your product upon upgrading and checking it.
    It will take 10 working days or more for upgrading (except for the transportation period).

  4. Effective Date of Application
    From July 1, 2002, to June 30, 2003, inclusive
    (If circumstances prevent you from sending your product within the above date, please contact your local Renesas Technology sales office or distributor.)

  5. Notices
    (1) If your probe does not work properly, a charge will be made for repairing it.
    (2) We will not be able to supply you with another probe for the upgrade.




© 2008. Renesas Technology Corp., All rights reserved. Privacy | Legal