Tool News
 
 
 

Tool News

Products Info
Downloads
Tools FAQs
MAEC TOOL NEWS: MAECT-M3T-MR308-020716D

A Note on Real-Time OS
M3T-MR308

Please take note of the following problem in using real-time OS M3T-MR308 for the M32C/80 and M16C/80 series MCUs:
  • On limitations imposed when M3T-MR308 is used for the M32C/82 and 83 group MCUs


  1. Versions Concerned
    All the versions of M3T-MR308

  2. Descriptions
    The following limitations are imposed when M3T-MR308 is used for the M32C/82 and 83 group MCUs:
    (1) Time intervals of timer interrupts the system timer can use must satisfy the condition below.
    A time interval of timer interrupts x clock frequency <= 65535 x 8
    For example, when the system is operating at a clock frequency of 20 MHz, each time interval of timer interrupts must be equal to or less than 26.214 ms.

    (2) If intelligent I/O interrupt 11 or CAN interrupt 2 is used, the following functions are disabled:
    • Mailbox function (only when message size is 32 bits long)
    • Variable-length memory pool function

  3. Schedule of Fixing the Problem
    We plan to fix limitation (2) above in our next release.




© 2008. Renesas Technology Corp., All rights reserved. Privacy | Legal